Technical FAQs

Ask a Question

How can I choose a NEMA rated Enclosed Safety Switch Disconnector from the Square D offer?

With reference to page # 3 in the attached Enclosed Safety Switch Disconnector catalogue, it is required to specify the following:
  1. Type of switch
  2. Pole configuration
  3. Voltage rating
  4. Ampere rating
  5. Availability of Neutral
  6. NEMA Enclosure type to which the switch is enclosed
  7. Any special requests or factory modifications to be carried out on the standard product

Accordingly, and in most cases, user could compile the reference according to his requirement.
Was this helpful?
What can we do to improve the information ?