Technical FAQs

Ask a Question

What is the part number for the CanOpen cable to fit the ATV312 drives?

Issue:
Customer is looking for the CanOpen cable to connect the daisy chain on the ATV312 drives with the VW3A31208 daisy chain card

Product line:
ATV312, Altivar 312

Environment:
all

Cause:
Not listed in the Digest.

Resolution:
VW3CANCARR03 is a 0.3 meter cable.
VW3CANCARR1 is a 1 meter cable.

More cable accessories and options are listed in the ATV312 catalog.  Document # DIA2ED2090-404EN

 
Was this helpful?
What can we do to improve the information ?