Technical FAQs

Ask a Question

What is a A136 Option on a 58M enclosed drive?

Issue:
What is a A136 Option on a 58M enclosed drive?

Product Line:
ATV58 drives

Environment:
58M enclosure

Cause:
A136 option

Resolution:
Here is the response from Seneca:
 
A136 stands for Mods A10, 110, 310 and 610.
 
A10 - 5% Line Reactor
110 - Additional Control Power VA Transformer
310 - Order contains E-Mods or Special Modifications (added by the engineer)
610 - ID Engraved Enclosure Nameplates
E228 - Motor Over Temperature Logic
SPL1 - Low Level Cut-off with Lights
 
 
Was this helpful?
What can we do to improve the information ?