Technical FAQs

Ask a Question

What is the default login ID and password for the Altivar Process webpage?

Issue:
What is the default login ID and password for the Altivar Process webpage?

Product Line:
Altivar Process drive
ATV630, ATV650

Environment:
All models, All serial numbers

Cause:
Customer is unable to log on to the webpage of the drive, it is requesting login credentials and they do not know the correct user ID or password.

Resolution:
The Default login ID is ADMIN.  
The Default Password is ADMIN.  
You will be prompted to change the login ID and password when you connect to the webpage the first time.

If this does not work, then someone has already changed the login and password.  Contact the person responsible for this.
Was this helpful?
What can we do to improve the information ?