Technical FAQs

Ask a Question

Wiser Air HVAC System Compatibility

Issue:
HVAC system compatibility for Wiser Air thermostat

Product Line:
Wiser Air

Environment:
Applies to Wiser Air thermostats only.

Cause:
While Wiser Air is compatible with most common HVAC systems, there are some exceptions.

Resolution:
Wiser Air is compatible with forced air, radiant, heat pump (including geothermal), oil, gas and electric systems.
It will also support up to 3 stages of heating and up to 2 stages of cooling.
Was this helpful?
What can we do to improve the information ?