Technical FAQs

Ask a Question

What is TCP/IP?

Issue:
Is TCP/IP a type of communication protocol?

Product Line:
Smart Systems

Resolution:
Smart Systems utilizes Modbus TCP/IP as an Ethernet communication protocol.

TCP/IP - Transmission Control Protocol - Internet Protocol is the protocol or language computers use to communicate and travel on the internet.
 
  • TCP - Transmission Control Protocol is responsible for breaking data down into small packets before they can be sent over a network, and for assembling the packets again when they arrive.
  • IP - Internet Protocol - takes care of the communication between computers. It is responsible for addressing, sending and receiving the data packets over the Internet.
  • Modbus TCP/IP - This is a Modbus variant used for communications over TCP/IP networks (Ethernet). 
Was this helpful?
What can we do to improve the information ?