Technical FAQs

Ask a Question

What is the IFE Switchboard Server (LV434011)?

Product Line:
Smart Systems

Resolution:
Same as IFE Module plus:
IFE Switchboard Server (LV434011) adds a Modbus serial input and supports the stacking of up to 12 IFMs for the input of RS485 Modbus connections. (Note –The IFE Web pages support up to 13 total devices, however the IFE can support the throughput of up to 20 serial devices.  Each IFE supports only one ULP connection) 
 
Was this helpful?
What can we do to improve the information ?