Technical FAQs

Ask a Question

What is the IFM Module (TRV00210)?

Issue:
What does the IFM do?

Product Line:
Smart Systems

Resolution:
Interface Modbus (IFM) Module allows connection of a breaker ULP connection to the Modbus serial network. 
 
Note: The IFM enables TCP/IP connectivity to all ULP & Modbus devices connected to itself with the help of IFE Switchboard Server (LV434011).   

 
Was this helpful?
What can we do to improve the information ?