Technical FAQs

Ask a Question

What are the I/O Module Functions?

Issue:
How is the IO Module used?

Product Line:
Smart Systems

Resolution:
The Input/Output Module is used for physical input and output connections to various devices.  It serves as the cradle communications module for Low Voltage Drawout circuit breakers (LVDO), drives pilot lights, etc.  The I/O module communicates via ULP cable to either an IFE or IFM to connect to external system
 
Was this helpful?
What can we do to improve the information ?