Technical FAQs

Ask a Question

What is the Front Display Module (FDM128)?

Product Line:
Smart Systems

Resolution:
The FDM128 is a preconfigured color touch screen which displays Micrologic metering, alarms, and operating information via a touch screen menu.  The FDM128 monitors and controls up to 8 circuit breakers.  The FDM128 auto-discovers up to 8 supported devices.
 
Was this helpful?
What can we do to improve the information ?