Technical FAQs

Ask a Question

Why is my Wiser Air inside temperature not accurate.

Wiser Air
The Wiser Air thermostat takes about 6 minutes to calibrate all 3 temperature sensors after booting up. If display is on for a long time or performing a firmware update will cause the temperature of the internal circuitry to rise. In result, this will cause the thermostat to think the room temperature is higher causing a delay for heating or excessive cooling. If the thermostat is exposed to direct sunlight or near an air return can also affect the temperature readings as well. 
Was this helpful?
What can we do to improve the information ?