Technical FAQs

Ask a Question

When using limit switch function on the ATV312, can the limit switch contacts be normally open?

Issue:
When using limit switch function on the ATV312, can the limit switch contacts be normally open?

Product Line:
ATV312

Environment:
All 

Cause:
ATV312 limit switch function

Resolution:
No. The limit switch contacts must be normally closed. The stop is performed when the input is in state 0. The direction of operation is authorized in state 1
Was this helpful?
What can we do to improve the information ?