Technical FAQs

Ask a Question

Wiser Air thermostat will turn on after installation.

Product Line:
Wiser Air thermostat
Resolution:
  • Check your load center to confirm that your HVAC breakers are turned on and not in the off or tripped positions.
  • Wiser Air requires a 24 VAC and common from the heating or cooling system control board. If your previous thermostat did not have a common wire connected to the C terminal or any extra wires present, the wire extender will need to be installed. Please see the Wiser Air Installation Guide below for further help.
  • Be sure to not power the thermostat directly to 120/240 Vac. 
Was this helpful?
What can we do to improve the information ?