Technical FAQs

Ask a Question

Can the halo color be customized on Wiser Air?

Product Line:
Wiser Air thermostat
Resolution:
No. The halo colors are set to signify the mode/ status of your thermostat. The colors associated with the modes are as follows: Heating Mode = yellow, Cooling Mode = blue, Off = white, and Demand Response  (depending on your local utility) = red. When your system is running the halo will pulsate slowly.
  • The halo intensity can be configured by tapping on menu
  • Select Settings
  • Select Display
  • Then adjust the slider to your desired Halo Intensity.
Was this helpful?
What can we do to improve the information ?