Technical FAQs

Ask a Question

Not receiving the verification code, What should I do?

Product Line:
Wiser Air 
Resolution:
If the email of verification code is not received , the code could be at the spam folder or the customer email address may be over quota. 
Another reason could be that the customer is not able to receive emails from our system.  After testing all the steps listed, and if the verification code is still not received, customer may need to try with another email address. For further assestance contact technical support at (855) 559-4737 or email wiser_support@schneider-electric.com.
 
Was this helpful?
What can we do to improve the information ?