Technical FAQs

Ask a Question

How to add a second Wiser Air thermostat to an existing account?

From the online account:
1. Log into the online account.
2. Click on the top right primary account holders name.
3. Next go to Profile & Settings.
4. Scroll down to Devices & Device Permissions
5. Click + Sync Devices.
6. Add a Device Name & Enter the Wiser Code (catchphrase)
 
From the App:
 
Android:
  • Menu -> Settings -> Sync Device -> Add a Device Name & enter the code or scan the QR Code by pressing the camera.
IOS:
  • Menu -> Settings -> Sync Device -> Add a Device Name & enter the code or scan the QR Code by pressing the camera.
 
 
Was this helpful?
What can we do to improve the information ?