Technical FAQs

Ask a Question

Can the bus on the ATV630 process drives be shared?

Issue:
Common Bus application with the ATV630 Process drives

Product Line:
ATV630

Environment:
All models and serial numbers

Cause:
None

Resolution:
No, the ATV630 was not designed to share the bus on two or more drives.
Was this helpful?
What can we do to improve the information ?