Technical FAQs

Ask a Question

Extra Two Stabs on the LR2K Overloads

Issue:
What are the extra two stabs used for on the LR2K overloads?

Product Line:
IEC Overload Relays - GIC Product

Environment:
US Product

Cause:
Product Characteristics

Resolution:
These stabs integrate with the coil and the NO contact on the single contactor that this unit is joined with to simplify wiring for a traditional three-wire control scheme.  Reference the attached document for further information.
Was this helpful?
What can we do to improve the information ?