Technical FAQs

Ask a Question

Tesys D-Line Maximum Hz Voltage for Power Poles

Issue:
What is the maximum Hz voltage that can be applied to the Tesys D-line contactors?

Product Line:
IEC Contactors - GIC Product

Environment:
US Product

Cause:
Product Characteristics

Resolution:
These units have been tested for frequencies 25Hz to 400hz within the operational current of the device .  No testing has been done beyond this frequency.
Was this helpful?
What can we do to improve the information ?