Technical FAQs

Ask a Question

How can I get a Nema 1 rating for an ATV312 drive?

issue:
How can I get a Nema 1 rating for an ATV312 drive?

Product Line:
ATV312 

Environment:
All 

Cause:
Mounting the drive externally 

Resolution:
Installation of a Conduit Entrance kit and retention of vent cover on top of drive controller provides the ATV312 with UL Type 1 rating.
Was this helpful?
What can we do to improve the information ?