Technical FAQs

Ask a Question

What can I use to change the settings on devices in my Conext system?

Issue:
Customer would like to know what devices can be used to change settings in a Conext system.

Product Line:
Conext XW+, Conext SW, Conext XW

Environment:
All models

Cause:
N/A

Resolution:
The three primary options for changing settings in a Conext system are a Conext System Control Panel, Conext ComBox, or Conext Configuration Tool.
  • The System Control Panel (SCP) is a graphical display that communicates over the Xanbus network and is local to the system.
  • The ComBox is a network enabled device that allows remote changes to the system through a TCP/IP network connection and web browser on a computer.
  • The Config Tool is a Xanbus to USB adapter that allows a computer to communicate with a Conext system through the XW Config software
Was this helpful?
What can we do to improve the information ?