Technical FAQs

Ask a Question

What does it mean when my ATV312 drive shows an "888" error code?

Issue:
,What does it mean when my ATV312 drive shows an "888" error code?

Product Line:
ATV312 Drives

Environment:
All serial numbers for ATV312 Drives

Cause:
N/A

Resolution:
"888" is not an error message, but means that the led light is illuminated. 
Try to power cyle the drive
Replace the drive
Was this helpful?
What can we do to improve the information ?