Technical FAQs

Ask a Question

What is the wire range for the terminal provided on the Electrical Interlock Kits used with safety switches?

Product Feature

Product Line:
HD SS Accessory

Wire range of terminals

The Electrical Interlock Kits use either the 9007AO1 snap switch (1NO/1NC contacts) or 9007CO3 snap switch (2NO/2NC contacts). The terminals provided on these snap switches accept #22 - #14 AWG wire. 
Was this helpful?
What can we do to improve the information ?