Technical FAQs

Ask a Question

What is the password for the Altivar process drive's webserver?

Issue:
What is the password for the Altivar process drive's webserver?

Product Line:
Altivar Process

Environment:
All

Cause:
First time login or need to reset.

Resolution:
By default the user name is ADMIN and the password is also ADMIN. During first time login, these will need to be changed. To reset to the default login requires a reset of the webserver configuration.  Go to My Preferences /  Webserver, then to Reset EmbWeb and change to yes.
Was this helpful?
What can we do to improve the information ?