Technical FAQs

Ask a Question

What parts are needed to mount the XVC4 on top of a cabinet?

Issue:
What part# do you need to mount the XVC4 on top of a Cabinet

Product Line:
XVC 

Environment:
Stacklights

Resolution:
Base mounted units can be direct mounted to the top of an enclosure. For mounting of the Support tube units the following can be used. 
Either the XVCZ11 Die-cast metal mounting base (for use with XVC4•• and XVC4••5S with support tube), 
or the XVCZ01 Plastic mounting base (for use with XVC4, XVC4•• and XVC4••5S — customer must discard the support tube) can be used
Was this helpful?
What can we do to improve the information ?