Technical FAQs

Ask a Question

What is the range of "Rated Motor Current" (NCR) of the ATV61 and ATV71 series drives?

Issue:
What is the range of "Rated Motor Current" (NCR) of the ATV61 series drives?

Product Line:
ATV61, ATV71

Environment:
All models, All serial numbers

Cause:
Customer wants to run an undersized motor on an ATV61 or 71 series drive but does not know the minimum size allowed

Resolution:
The Rated Motor Current setting of the ATV61/ATV71 series drives can be set anywhere between .25 and 1.1 times the nominal rating of the drive itself, as found on the nameplate of the drive.
Was this helpful?
What can we do to improve the information ?