Technical FAQs

Ask a Question

How do I set up my ATV12 drive to be controlled by the remote keypad (VW3A1006 or VW3A1007)?

Issue:
Wants to control the VFD using the remote keypad.

Product Line:
Altivar 12, ATV12

Environment:
All model numbers.  
Requires VW3A1006 or VW3A1107 remote keypad display and cable

Cause:

Resolution:
Go to the FULL menu and the CtL submenu.
Set Fr1 to LCC.
Make sure CHCF is set to SIn.

After cycling power to the drive the remote keypad should be active for both Speed control and Start/Stop.
 
Was this helpful?
What can we do to improve the information ?