Technical FAQs

Ask a Question

Can Bolt-Loc switch contacts can be visually seen in the open position to confirm they are open?

Issue:
Can BP Bolt-Loc switch contacts can be visually seen in the open position to confirm they are open?

Product Line:
QED SWBD with BP Main Switches

Environment:
Specifications

Cause:
Product Features

Resolution:

A Viewing Window can be selected when designing SWBD that will allow the blades to be seen in the open positon, but will not allow sight of the opening gap.
There is a kit for the 800-2000 amp switches to allow sight of the gap as well.

 
Was this helpful?
What can we do to improve the information ?