Technical FAQs

Ask a Question

What does form VZ4 mean in relation to a 9012ACW?

Issue:
What is VZ4 in 9012ACW

Product Line:
9012ACW

Environment:
Pressure Switch

Resolution:
The VZ4 at the end of the 9012ACW number was a seal cap and lock nut on the range adjustment to lock that adjustment to passers-by. The GAW has all the adjustments behind the cover so VZ4 is not required. Form Z would change the connection threading, should not be used.
Was this helpful?
What can we do to improve the information ?