Technical FAQs

Ask a Question

Does setting RPM value matter in the ATV71/ATV61 drive or is it used just for displaying motor speed?

Issue:
Does setting RPM value matter in the ATV71/ATV61 drive or is it used just for displaying motor speed?

Product Line:
ATV61 ,ATV71

Environment:
All

Cause:
N/A

Resolution:
Motor RPM or the Nominal Speed does tell the drive something about the motor characteristics i.e. how much slip it has at Full Load.

 
Was this helpful?
What can we do to improve the information ?