Technical FAQs

Ask a Question

What are the repair parts for a CHU366AWK Series E6 (or E06) Heavy Duty Safety Switch?

Current Design Repair parts

Product Line:
Canadian Heavy Duty Safety Switches

Repair Parts


NOTE: This is a Non-Fusible Switch so it does NOT have a Separate Load Base Assembly.

The parts listed here are the only field replaceable parts.

Line-Load base assembly - 4055270451 (3-required and includes the arc suppressor assembly)
Arc suppressor assembly - 4051270850 (3-required)
Lug assembly - 4025113650 (4 required per base assembly)
Line base phase insulator - 4055219301 (2 required)
Line-Load base mounting screws - 4020600901 (3 required per base assembly)
Handle assembly - 4051217251
Handle assembly mounting screw and washer - 2140122242 (Screw 2 required) and 2370100220 (washer 2 required)
Door thumb retainer - 4405043301
Door thumb screw - 4405043401 
Handle knob kit - 40283-435-50 (the black & red knob at the end of the handle)
Cross Bar Insulator - 4055217801 ( 1 required the insulator is Red, approx. 8.85" in length and 1.46" wide)
Cross Bar Insulators - 4055217701 (2 Required, these insulators are Red, approx. 4.16" in length and 2.5" in width) 
Dust Shield - 4055215701 (1 require, this part is Red in color and approx. 16.1" in length and 1.16" in width)
Was this helpful?
What can we do to improve the information ?