Technical FAQs

Ask a Question

What is the rise time (slew rate) of the PWM output signal of an ATV312 series drive?

Issue:
What is the rise time (slew rate) of the PWM output signal of an ATV312 series drive?

Product Line:
ATV312 series drives.

Environment:
All models, All serial numbers, Any switching frequency rate

Cause:
Customer has a motor that requires a DV/DT filter if the rise time is less than 2 microseconds but this information is not available in current literature.

Resolution:
The Rise time of the 3 phase PWM output of the ATV312 series is 0.1 microseconds.  This is not significantly affected by changes in switching frequency.
Was this helpful?
What can we do to improve the information ?