Technical FAQs

Ask a Question

Do you offer a 120Vac adapter for the logic input for the ATV312?

Issue:
Do you offer a 120Vac adapter for the logic input for the ATV312?

Product Line:
Variable Frequency Drives

Environment:
Applies to ATV12, ATV312, ATV61, ATV71

Cause:
Customer looking for a drive that can accept 120Vac signal on its logic inputs

Resolution:
There is no option card available for the ATV12 or ATV312 to make the logic inputs 120Vac
It is ONLY available for the ATV61 or ATV71 part number VW3A3101

Keywords:
120V adapter
Was this helpful?
What can we do to improve the information ?