Technical FAQs

Ask a Question

Why does the 2012 ATV312 Annex show circuit breakers for the single-phase 230v drives and the 2014 Annex does not show them?

Issue:
Why does the 2012 ATV312 Annex show circuit breakers for the single-phase 230v drives and the 2014 Annex does not show them?

Product Line:
ATV312 drives 

Environment:
230vac single-phase

Cause:
Why does the 2012 ATV312 Annex show circuit breakers for the single-phase 230v drives and the 2014 Annex does not show them?

Resolution: 
It was dropped by accident. It will be added again in the next ATV312 Annex update. 
Was this helpful?
What can we do to improve the information ?