Technical FAQs

Ask a Question

What is Front Display Module (FDM121)?

Product Line:
Modbus accessories

Resolution:
The FDM121 (catalog number STRV00121) is a preconfigured unit for displaying Micrologic metering, alarms, and operating information. The FDM121 monitors one breaker.  It can display data and reset accumulated and min/max values.  It CANNOT be used to change any breaker protective settings.


 
Was this helpful?
What can we do to improve the information ?