Technical FAQs

Ask a Question

How Can I Obtain a Modbus RS485 Connector for my Communications Gateway

Question:

I lost my Modbus connector for the Xanbus Communications Gateway.  Do you know one I can use?

Answer:

A common Modbus connector to use is from Phoenix Contact.  Please see the attached file for more information on the connector.

http://www.newark.com/phoenix-contact/mstb-2-5-4-st/terminal-block-standard-4way-24/dp/88W5006?CMP=KNC-GUSA-GEN-SHOPPING-NEW-PHOENIX-CONTACT&ad=81515568741&gclid=CNGN7oPPyssCFRSPfgod2BICOQ

Disregard image in the link, it is provided only as an example.

 
Was this helpful?
What can we do to improve the information ?