Technical FAQs

Ask a Question

How is the Process drive put into local keypad control​?

Issue:
How is the Process drive put into local keypad control​?

Product Line:
Process Drives

Environment:
All models and serial numbers

Cause:
The Local/Remote key does nothing.

Resolution:
The function of the Local/Remote key first needs to be enabled by going to the Complete Settings menu, then Command and Reference.  Scroll down to HMI Command and enable it by selecting Stop or Bumpless depending on the preferred action when switching to Local mode.

Was this helpful?
What can we do to improve the information ?