Technical FAQs

Ask a Question

Is the ATV660 process drive available for 208V 3 phase input?

Issue:
Is the ATV660 process drive available for 208V 3 phase input?

Product Line:
ATV660 enclosed process drive system.

Environment:
All

Cause:
Current literature is vague.

Resolution:
Yes, the 230V (U3) version of the ATV660 process drive system can also operate at 208V.   Standard offering is 208/230V and 460V.  Other input voltage options are available upon request.  When programming motor data into the drive, be sure to use the correct data to match the input voltage of the drive.
Was this helpful?
What can we do to improve the information ?