Technical FAQs

Ask a Question

With a ATV71 encoder card, what is the scan time of the speed regulation control loop?

Issue:
With a ATV71 VW3A3401 encoder card, what is the scan time of the speed regulation control loops?

Product Line:
All ATV71 drives

Environment:
All encoder cards

Cause:
Speed regulation

Resolution:
The application task is running at one millisecond. 

So the reference speed from the application is updated each millisecond. 

Also the inputs or outputs of the drive are refreshed at the same time. 

 


 
Was this helpful?
What can we do to improve the information ?