Technical FAQs

Ask a Question

Can a VFD control the speed of a motor when running in bypass?

Issue: 
Can a VFD control the speed of a motor when running in bypass?
 
Product Line:
EFLEX, MFLEX, SFLEX, ECONOFLEX, CPD
 
Environment:
All enclosed units with bypass
 
Cause:
N/A
 
Resolution:
When running in bypass, the motor is running directly from line power, the VFD has no control of the motor.           
 
Was this helpful?
What can we do to improve the information ?