Technical FAQs

Ask a Question

What are the dimensions for the HCW86D door kit?

Issue:
What are the dimensions for the HCW86D door kit?

Product Line:
Panelboards

Environment:
I-line panelboards

Cause:
product features

Resolution:
This door is a double "saloon" style door.  Each door is 61.60" x 16.62".
Was this helpful?
What can we do to improve the information ?