Technical FAQs

Ask a Question

What is the address of the command word of the ATS48?


Issue: 
What is the address of the command word of the ATS48?
 
Product Line:
Altistart 48
 
Environment:
All serial numbers
 
Cause:
N/A
 

Resolution:
The Modbus command word address for the ATS48 is 400.  However, Modbus requires an offset.   If the controller does not have a built in offset, then the actual value you would enter would be 401.              
 
Was this helpful?
What can we do to improve the information ?