Technical FAQs

Ask a Question

Why can the rFC function assignment not be changed in the ATV32?

Issue: 
Why can I not assign rFC function to LI2 in the ATV32?

Product Line:
ATV32

Environment:
All
 
Cause:
Installation / Setup

Resolution:
The CHCF profile must be set to Seperate or IO and Access cannot be standard.  Increase access level.
Was this helpful?
What can we do to improve the information ?