Technical FAQs

Ask a Question

Is the cable and remote mounting hardware include with the ATV61 / ATV71 drives? 

Issue: 
ATV61 is missing the cable and mounting kit.

Product Line:
ATV61 ATV71

Environment:
All
 
Cause:
Delivery or Collection Issues

Resolution:
Mounting kit VW3A1102  is not included. 
Cables   VW3A1104Rxx  is not included. 
 
Was this helpful?
What can we do to improve the information ?