Technical FAQs

Ask a Question

Can the ATV32 be programmed for multiple sets of motor parameters?

Issue:
Can the ATV32 be programmed for multiple sets of motor parameters?

Product Line:
ATV32 series drives

Environment:
All models, All serial numbers

Cause:
Customer needs clarification

Resolution:
Yes, It is possible to program up to three sets of motor parameters into the ATV32 series drives and switch between them via logic input.    For more detailed information, please refer to pages 227 through 230 of the attached ATV32 programming manual. 
 
Was this helpful?
What can we do to improve the information ?