Technical FAQs

Ask a Question

Are there any reset operators for the 30mm series

Issue:
Are there any reset operators for the 30mm series

Product Line:
9001 K and SK

Environment:
Pushbuttons

Resolution:
We do not have a 9001K or 9001SK marked as a reset operator, these are only available in the 22mm line.
We do have the 9066R kits offered in the NEMA line that mount in a 30 mm hole, including the 9066RA1 with one rod, 9066RA2 with 2 rods, and 9066RA3 with 3 rods intended for use in OEM kits for commercial enclosures. 
Was this helpful?
What can we do to improve the information ?