Technical FAQs

Ask a Question

Where do I wire my Run and Trip Status Contacts for an ATS22 Enclosed with Mods F10 and J10?

Issue:
Where do I wire my run and trip status contacts for an ATS22 Enclosed with mods F10 and J10?

Product Line:
ATS22 Enclosed

Environment:
All products of ATS22 Enclosed

Cause:
N/A

Resolution:
Run contacts are wired on 5 and 6
Trip status on 40 and 41
Run status on 52 and 53 (Normally Open)


 
Was this helpful?
What can we do to improve the information ?