Technical FAQs

Ask a Question

What are the dimensions of the ground bar, part number GLK12 used in Stab-Lok loadcentres?

Issue:
What is the GLK12 dimensions?

Product Line:
Stab-Lok Loadcenters

Environment:
Dimensions

Cause:
Installation

Resolution:
The GLK12 Stab-Lok Ground bar is approximately 5.0" Long x 0.437" Height x 0.312" Width.
 
Was this helpful?
What can we do to improve the information ?