Technical FAQs

Ask a Question

What is the replacement board set for the RAM DBS and DBS II?

Issue:
What is the part number for the RAM DBS and DBS II replacement board set?

Product Line:
DBS and DBS II

Environment:
All models

Cause:
None

Resolution:
The replacement board set is RAM-400339-AF.

If the existing board set is the older green circuit board version, pre-10/18/2004, then several modifications are required. Order the conversion kit, RAM-400339-KIT.  It includes:
RAM-400339-AF circuit board set
WC-0040 display cable
TB-0206 TB2 CT connector
Instructions - see attachment below
 
Was this helpful?
What can we do to improve the information ?