Technical FAQs

Ask a Question

Are time stamps for past fault codes available on the ATS22 and ATS48 soft starts?

Issue:
Are time stamps for past fault codes available on the ATS22 and ATS48 soft start?

Product Line:
Altistart 48, Altistart 22

Environment:
All

Cause:
N/A

Resolution:
Unfortunately,  there is no time stamp function available for past error codes on the ATS22 or ATS48 soft starts.
Was this helpful?
What can we do to improve the information ?